DOCA0006EN-08

Meter sealing points

All meters have sealing covers and three sealing points to help prevent access to inputs, outputs, current, and voltage connections.

 

A

Sealing points (3)

 

B

Sealable covers (2)

 

NOTE: The sealable covers must be installed and sealed to the sealing points with the steel cable. Use steel cable with 1.6 mm (1/16 in) diameter and 152.4 mm (6 in) adjustable length for sealing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.