DOCA0006EN-08

Quick response code

A Quick Response Code (QR Code) is a type of matrix barcode used to store data efficiently.

You can view energy values and read data by scanning the QR Code displayed on the meter screen. The dynamically generated QR Code contains a URL that represents the meter’s data.

The URL provides basic configuration information about the meter, including power system, and communication configuration. Other parameters such as product reference, serial number, and firmware version are also included as elements in the URL.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.