DOCA0006EN-08

Set External Control from Digital Output (PM3255)

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

21000

W

1

UInt16

(Reserved)

W

1

UInt16

1, 2

Digital output ID

  • 1 = DO1
  • 2 = DO2

W

1

UInt16

0, 1

Digital output status

  • 0 = Open
  • 1 = Close

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.