DOCA0006EN-08

Set Digital Input as Partial Energy Reset (PM3255)

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

6017

W

1

UInt16

(Reserved)

W

1

UInt16

0 – 3

Digital input to associate:

  • 0 = None
  • 1 = DI1
  • 2 = DI2
  • 3 = DI1 and DI2

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.