DOCA0006EN-08

Input Metering Setup

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

PM3250

PM3255

Input Metering Channel 01

0x1B77

7032

R/WC

20

UTF8

Label

0x1B8B

7052

R/WC

2

Float32

pulse/unit

Pulse Frequency

0x1B8E

7055

R/WC

1

UInt16

Digital Input Association:

  • 0 = DI1 disable for input metering
  • 1 = DI1 enable for input metering

Input Metering Channel 02

0x1B8F

7056

R/WC

20

UTF8

Label

0x1BA3

7076

R/WC

2

Float32

pulse/unit

Pulse Frequency

0x1BA6

7079

R/WC

1

UInt16

Digital Input Association:

  • 0 = DI2 disable for input metering
  • 2 = DI2 enable for input metering

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.