DOCA0006EN-08

Other Characteristics

The following table lists other characteristics of the meter:

Characteristics

Description

Reset

Epart

Per phase, partial, by tariff energy values

Minimum and maximum values

Peak demand values

Local or remote setup

Distribution system type

Three-phase 3-wire or 4-wire with 1, 2, or 3 CTs

Single-phase 2-wire or 3-wire with 1 or 2 CTs, with or without VTs

Current transformers rating

Primary 5 to 32767 A

Secondary 5 A, 1 A

Voltage transformers rating

Primary 1000000 Vmax

Secondary 100, 110, 115, 120

Current demand calculation method

1 to 60 minutes

Power demand calculation method

1 to 60 minutes

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.