DOCA0006EN-08

Multi-tariff

The meter provides multi-tariff energy accumulation. It supports up to 4 tariffs.

The tariff switching has the following 3 kinds of control modes:

  • Digital input

  • Communication

  • Internal real-time clock (RTC)

You can configure the control mode by using the display (all the 3 modes) or by using communication (not for RTC).

Command number 2060 is used to configure the control mode by communication. Refer Communication using Modbus section for more details.

The following table presents the rules to change multi-tariff control mode by Modbus command:

From

To

Disable

Communication

Digital input

RTC

Communication

Communication

Disable

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.