DOCA0006EN-08

Demand System Setup

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

2002

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

1, 2

Demand method:

  • 1 = Timed interval sliding block
  • 2 = Timed interval fixed block

W

1

UInt16

min

10, 15, 20, 30, 60

Demand interval duration

W

1

UInt16

(Reserved)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.