DOCA0006EN-08

Set Wiring

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

2000

W

1

UInt16

(Reserved)

W

1

UInt16

1, 3

Number of phases

W

1

UInt16

2, 3, 4

Number of wires

W

1

UInt16

0, 1, 2, 3, 11, 13

Power System Configuration:

  • 0 = 1PH2W L-N
  • 1 = 1PH2W L-L
  • 2 = 1PH3W L-L-N
  • 3 = 3PH3W
  • 11 = 3PH4W
  • 13 = 1PH4W L-N

W

1

UInt16

Hz

50, 60

Nominal Frequency

W

2

Float32

(Reserved)

W

2

Float32

(Reserved)

W

2

Float32

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

2

Float32

V

VT Secondary – 1000000.0

VT Primary

W

1

UInt16

V

100, 110, 115, 120

VT Secondary

W

1

UInt16

1, 2, 3

Number of CTs

W

1

UInt16

A

1 to 32767

CT Primary

W

1

UInt16

A

1, 5

CT Secondary

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

0, 1, 2

VT Connection type:

  • 0 = Direct Connect
  • 1 = 3PH3W (2 VTs)
  • 2 = 3PH4W (3 VTs)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.