DOCA0006EN-08

Real-time measuring

The following table lists the metering characteristics of the meter for the real-time measurement:

Characteristics

Description

Current

Per phase, neutral, and average of 3 phases

Voltage

L-L, L-N, and average of 3 phases

Frequency

40...70 Hz

Active power

Total and per phase (signed)

Reactive power

Total and per phase (signed)

Apparent power

Total and per phase

Power factor (True)

Total and per phase

0.000 to 1 (signed) by display

0.000 to 2 (signed) by communications

Tangent phi (Reactive factor)

Total

Current unbalance

Per phase, most unbalanced of 3 phases

Voltage unbalance

L-L, most unbalanced of 3 phases

L-N, most unbalanced of 3 phases

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.