DOCA0006EN-08

Set Tariff

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

2060

W

1

UInt16

(Reserved)

W

1

UInt16

0 – 4

Multi-tariff mode:

  • 0 = Disable multi-tariff
  • 1 = Use COM as tariff control (maximum 4 tariffs)
  • 2 = Use 1 digital input as tariff control (2 tariffs)
  • 3 = Use 2 digital inputs as tariff control (4 tariffs)
  • 4 = Use RTC as tariff control (maximum 4 tariffs)

2008

W

1

UInt16

(Reserved)

W

1

UInt16

1 – 4

Tariff:

NOTE: Only if multi-tariff is controlled by communications
  • 1 = T1
  • 2 = T2
  • 3 = T3
  • 4 = T4

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.