DOCA0006EN-08

Overview of meter functions

The PM3200 series meters provide accurate 3-phase electrical parameters monitoring.

Following are the meter models:

  • PM3200

  • PM3210

  • PM3250

  • PM3255

The meters provide the various measurement capabilities required to monitor an electrical installation such as current, voltage, power, power factor, frequency, and energy.

The key features of the meters are:

  • Electrical parameters monitoring such as I, In, U, V, PQS, E, PF, Hz

  • Power / current demand, peak demand

  • Time-stamped alarms

  • Minimum/maximum values for many parameters

  • Management of up to 4 tariffs

  • Up to 2 digital inputs and 2 digital outputs

  • Modbus communication

  • QR codes with embedded data for viewing meter information using Meter Insights

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.