DOCA0006EN-08

Digital Inputs

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

PM3250

PM3255

0x1C69

7274

R

1

UInt16

Digital Input 1 Control Mode:

  • 0 = Normal (Input Status)
  • 2 = Multi-tariff Control
  • 3 = Input Metering
  • 5 = Energy Reset (Partial Energy, Energy by Tariff, Phase Energy)

0x1C81

7298

R

1

UInt16

Digital Input 2 Control Mode

0x22C8

8905

R

2

Bitmap

Digital Input Status:

  • 0 = Relay-Open
  • 1 = Relay-Closed
  • Bit 1 = DI1 status
  • Bit 2 = DI2 status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.