DOCA0006EN-08

DI control mode (PM3255)

In the DI control mode, the tariff switching is triggered by the change in input status of DI. Refer Digital inputs (PM3255) for more details.

NOTE:
  • If you change DI mode to other operation modes (normal input status, input metering, or energy reset) while multi-tariff control mode is in DI control mode, the multi-tariff function is automatically disabled.

  • If you change multi-tariff control mode to other control modes (communication or internal RTC) while DI is configured for multi-tariff function, the DI operation mode automatically changes to normal input status.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.