DOCA0006EN-08

Alarm Setup

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

7000

W

1

UInt16

(Reserved)

W

1

UInt16

PM3250 :
1, 6, 8, 9, 11, 30

PM3255 :
1, 2, 5 – 16, 19, 28, 30 – 32, 41

Alarm ID

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

0, 1

  • 0 = Disable
  • 1 = Enable

W

2

Float32

Alarm ID 1, 2, 5, 6, 7, 8, 11, 19: 0.0 – 9999999.0

Alarm ID 9, 10, 16, 30: -9999999.0 – 9999999.0

Alarm ID 12, 13: -2.0 – 2.0

Alarm ID 28, 31, 32: 0.0 – 1000.0

Alarm ID 41: 0 – 999999999

Pickup setpoint

W

2

UInt32

(Reserved)

W

2

Float32

(Reserved)

W

2

UInt32

(Reserved)

W

1

UInt16

(Reserved)

W

4

UInt16

(Reserved)

W

1

UInt16

(Reserved)

W

1

UInt16

(Reserved)

20000

W

1

UInt16

(Reserved)

W

2

Float32

0.0 – 99.0

Dropout setpoint

W

2

UInt32

0 – 999999

Trip time delay

W

1

Bitmap

0, 1, 2, 3

PM3250 : Reserved

PM3255 : Digital output to associate

  • 0 = None
  • 1 = DO1
  • 2 = DO2
  • 3 = DO1 and DO2

20001

W

1

UInt16

(Reserved)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.