DOCA0006EN-08

Peak demand

In non-volatile memory, the meter maintains a maximum operating demand values called peak demand. The peak is the highest value (absolute value) for each of these readings since the last reset.

You can reset peak demand values from the meter display. You should reset peak demand after changes to basic meter setup such as CT ratio or power system configuration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.