DOCA0006EN-08

Set Flex Log

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

2052

W

1

UInt16

0 – 6

Flex log mode:

  • 0 = Disable
  • 1 = Peak demand
  • 2 = KWH_KVAH
  • 3 = KWH_KVARH
  • 4 = KVARH_KVAH
  • 5 = KWH_KW
  • 6 = KWH_KVA

W

1

UInt16

10, 15, 20, 30, 60

Flex log interval duration in minutes:

  • 10, 15, 20, 30, 60

W

1

UInt16

1, 2

  • 0 = Open
  • 1 = Close
NOTE: Applies only when flex log mode is set to peak demand

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.