DOCA0006EN-08

Communications

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

PM3250

PM3255

0x1963

6500

R

R

1

UInt16

Protocol

  • 0 = Modbus

0x1964

6501

R/WC

R/WC

1

UInt16

Address

0x1965

6502

R/WC

R/WC

1

UInt16

Baud Rate:

  • 0 = 9600
  • 1 = 19200
  • 2 = 38400

0x1966

6503

R/WC

R/WC

1

UInt16

Parity:

  • 0 = Even
  • 1 = Odd
  • 2 = None

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.