DOCA0006EN-08

Diagnostic codes

If the combination of the backlight and the error / alert icon indicates an error or an abnormal situation, navigate to the diagnostics screen and find the diagnostics code. If the problem persists after following the instructions in the table, please contact Technical Support.

Diagnostic code

PM3200

PM3250

PM3210

PM3255

Description

Possible solution

LCD display is not visible.

Check and adjust LCD contrast/backlight settings.

Push buttons do not function.

Restart the meter by power off and power on again.

101, 102

Metering stops due to internal error.

Total energy consumption is displayed.

Enter the Configuration mode and implement Reset Config.

201

Metering continues.

Mismatch between frequency settings and frequency measurements.

Correct frequency settings according to the nominal frequency of the network.

202

Metering continues.

Mismatch between wiring settings and wiring inputs.

Correct wiring settings according to wiring inputs.

203

Metering continues.

Phase sequence reverses.

Check wire connections or correct wiring settings.

205

Metering continues.

Date and time have been reset due to loss of power.

Set Date and time.

206

Metering continues.

Pulse is missing due to overload on energy pulse output.

Check the energy pulse output settings and correct if needed.

207

Metering continues.

Abnormal internal clock function.

Restart the meter by power off and power on again.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.