DOCA0006EN-08

China Standard Compliance

This product complies with the following standards in China:

BS/EN/IEC 61557-12 Electrical safety in low voltage distribution systems up to 1 000 V a.c. and 1 500 V d.c. - Equipment for testing, measuring or monitoring of protective measures - Part 12: Performance measuring and monitoring devices

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.