DOCA0006EN-08

Status information

The energy pulse LED on the front panel indicate the current status of the meter.

The icons in the following table indicate the LED state:

 

= OFF

= Flashing

= ON

Energy pulse LED

5000 flashes/kWh

Not counting

Energy pulse counting

Over-counting due to incorrect configuration or overload

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.