DOCA0006EN-08

Overview

The main title and the sub menu in full screen mode are hidden and the values are expanded to full screen.

The full screen mode is enabled by default. You can modify full screen enable/disable, auto scroll enable/disable, and auto scroll interval.

NOTE: When full screen mode is enabled, the backlight is always ON and when full screen mode is disabled, the backlight goes to power saving mode.

Full screen

Auto scroll

Auto scroll interval

Description

Enable

Disable

Any value

Fixed summary page at full screen mode.

Enable

Enable

Any value

Auto scrolling pages at full screen mode. The interval between any 2 scrolling pages is the value specified in seconds.

Disable

Full screen mode disabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.