DOCA0006EN-08

Input Metering Setup (PM3255)

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

6014

W

1

UInt16

(Reserved)

W

1

UInt16

1, 2

Input metering channel

W

20

UTF8

string size ≤ 40

Label

W

2

Float32

1 – 10000

Pulse weight

W

1

UInt16

(Reserved)

W

1

UInt16

Input metering channel 1: 0, 1

Input metering channel 2: 0, 2

Digital input association:

  • 0 = None
  • 1 = DI1
  • 2 = DI2

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.