DOCA0006EN-08

Meter description

PM3200 / PM3210

 

A

Control power input (L1, L2)

 

B

Display

 

C

Energy pulsing LED (for checking accuracy)

 

D

Pulse output (S0+, S0-) for remote transfer (only PM3210)

 

E

Cancellation

 

F

Confirmation

 

G

Up

 

H

Down

 

I

Current inputs (I1, I2, I3)

 

J

Voltage inputs (V1, V2, V3, Vn)

   
 
 
 

PM3250 / PM3255

 

A

Digital inputs x 2 (only PM3255)

 

B

Digital outputs x 2 (only PM3255)

 

C

Communication port

 

D

Communications LED (for communication diagnosis)

 

E

Energy pulsing LED (for checking accuracy)

 

F

Cancellation

 

G

Confirmation

 

H

Up

 

I

Down

 

J

Display

 

K

Current inputs (I1, I2, I3)

 

L

Control power input (L1, L2)

 

M

Voltage inputs (V1, V2, V3, Vn)

   
 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.