DOCA0006EN-08

Energy Log

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

PM3250

PM3255

Energy Log - Day

0xB21F

45600

R

1

UInt16

Enable/Disable:

  • 0x0000 = Disable
  • 0xFFFF = Enable

0xB220

45601

R

1

UInt16

Maximum Entry Number

0xB221

45602

R

1

UInt16

Current Entry Number

0xB222

45603

R

1

UInt16

Latest Entry ID

0xB223

45604

R

1

UInt16

Oldest Entry ID

0xB224

45605

R

4

Int64

Wh

Real-time Value of Current Day

0xB228

45609

R

4

DATETIME

Entry 001 Date/Time

0xB22C

45613

R

4

Int64

Wh

Entry 001 Value

0xB388

45961

R

4

DATETIME

Entry 045 Date/Time

0xB38C

45965

R

4

Int64

Wh

Entry 045 Value

Energy Log - Week

0xB390

45969

R

1

UInt16

Enable/Disable:

  • 0x0000 = Disable
  • 0xFFFF = Enable

0xB391

45970

R

1

UInt16

Maximum Entry Number

0xB392

45971

R

1

UInt16

Current Entry Number

0xB393

45972

R

1

UInt16

Latest Entry ID

0xB394

45973

R

1

UInt16

Oldest Entry ID

0xB395

45974

R

4

Int64

Wh

Real-time Value of Current Day

0xB399

45978

R

4

DATETIME

Entry 001 Date/Time

0xB39D

45982

R

4

Int64

Wh

Entry 001 Value

0xB431

46130

R

4

DATETIME

Entry 020 Date/Time

0xB435

46134

R

4

Int64

Wh

Entry 020 Value

Energy Log - Month

0xB439

46138

R

1

UInt16

Enable/Disable:

  • 0x0000 = Disable
  • 0xFFFF = Enable

0xB43A

46139

R

1

UInt16

Maximum Entry Number

0xB43B

46140

R

1

UInt16

Current Entry Number

0xB43C

46141

R

1

UInt16

Latest Entry ID

0xB43D

46142

R

1

UInt16

Oldest Entry ID

0xB43E

46143

R

4

Int64

Wh

Real-time Value of Current Day

0xB442

46147

R

4

DATETIME

Entry 001 Date/Time

0xB446

46151

R

4

Int64

Wh

Entry 001 Value

0xB4A2

46243

R

4

DATETIME

Entry 013 Date/Time

0xB4A6

46247

R

4

Int64

Wh

Entry 013 Value

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.