DOCA0006EN-08

Dismounting

  1. Use a flat-tip screwdriver (≤ 6.5 mm / 0.25 in) to lower the locking mechanism and release the meter.
  2. Lift the meter out and up to free it from the DIN rail.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.