DOCA0006EN-08

Overview

The meter provides setpoint-driven alarms. The alarms include:

Alarms

PM3210 / PM3250

PM3255

Standard alarms

Over Current, Phase

Under Current, Phase

Over Voltage, L-L

Under Voltage, L-L

Over Voltage, L-N

Under Voltage, L-N

Over Power, Total Active

Over Power, Total Reactive

Over Power, Total Apparent

Leading Power Factor, Total

Lagging Power Factor, Total

Over Demand, Total Active Power, Present

Over Demand, Total Apparent Power, Present

Over THD-U, Phase

Under Power, Total Active

Over THD-I, Phase

Over THD-V, Phase

Customized Alarms

Over Energy, Total Active

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.