DOCA0006EN-08

Reset Input Metering Counter (PM3255)

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

2023

W

1

UInt16

(Reserved)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.