DOCA0006EN-08

Digital Outputs

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

PM3250

PM3255

0x25C8

9673

R

1

UInt16

Digital Output 1 Control Mode Status:

  • 2 = Alarm
  • 3 = Energy
  • 0xFFFF = Disable

0x25D0

9681

R

1

UInt16

Digital Output 2 Control Mode Status

0x25C2

9667

R

2

Bitmap

Digital Output Status:

  • 0 = Relay-Open
  • 1 = Relay-Closed
  • Bit 1 = DO1 status
  • Bit 2 = DO2 status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.