DOCA0006EN-08

Minimum/Maximum values

When any one-second real-time reading reaches its highest or lowest value, the meter saves the minimum and maximum values in its nonvolatile memory.

From the meter display, you can:

  • View all minimum/maximum values since the last reset and the reset date and time

  • Reset minimum/maximum values

All running minimum/maximum values are arithmetic minimum and maximum values. For example, the minimum phase A-N voltage is the lowest value in the range from 0 to 1 MV that has occurred since last reset of the minimum/maximum values.

The meter provides time stamping for 6 minimum/maximum values.

The following table lists the minimum and maximum values stored in the meter:

Characteristics

Description

Current

Per phase, neutral, and average *

Minimum: lowest of 3 phases *

Maximum: highest of 3 phases *

Voltage

L-L and L-N per phase and average

Frequency

Active power

Per phase * and total

Reactive power

Per phase * and total

Apparent power

Per phase * and total

Power factor

Per phase * and total

Tangent phi (Reactive factor)

Total *

THD current (PM3210 / PM3250 / PM3255)

Maximum: Per phase, neutral, and highest of 3 phase *

Minimum: Per phase * and neutral *

THD voltage (PM3210 / PM3250 / PM3255)

L-L and L-N per phase *

Maximum: Highest of 3 phases *

Minimum: Lowest of 3 phases *

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.