DOCA0006EN-08

Energy readings

The meter calculates and stores total and partial energy values for active energy, reactive energy, and apparent energy.

You can view energy values from the display. The resolution of the energy value automatically changes from kWh to MWh (kVAh to MVARh).

The energy values automatically resets to 0 when it reaches the limit of 1 x 106 MWh, 1 x 106 MVAh, or 1 x 106 MVARh. Manual reset of total energy is not allowed. You can reset the partial energy values including partial energy import, energy by tariff, and phase energy manually using the display.

Energy values can be reported over communications as 64-bit signed integers. The units are always Wh, VARh, or VAh.

The following table lists the energy readings from the meter:

Characteristics

Description

Energy values (import)

Active energy

Total and per phase, partial, by tariff

0 to 1 x 1012 Wh

Auto reset to 0 in case of over limit

Reactive energy

Total and per phase, partial

0 to 1 x 1012 VARh

Auto reset to 0 in case of over limit

Apparent energy

Total and per phase, partial

0 to 1 x 1012 VAh

Auto reset to 0 in case of over limit

Energy values (export)

Active energy

Total

0 to 1 x 1012 Wh

Auto reset to 0 in case of over limit

Reactive energy

Total

0 to 1 x 1012 VARh

Auto reset to 0 in case of over limit

Apparent energy

Total

0 to 1 x 1012 VAh

Auto reset to 0 in case of over limit

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.