DOCA0006EN-08

Default configuration mode settings

Function

Factory settings

Wiring

3PH4W; VT Direction connection; 3 CTs on I1, I2, and I3

CT Ratio

CT Secondary = 5 A; CT Primary = 5 A

VT Ratio

NA

Nominal frequency

50 Hz

Nominal phase order

A-B-C

Date / Time

1-Jan-2000/00:00:00

Multi-tariffs

Disable

Demand

Method: sliding block; Interval: 15 minutes

Power demand log

Disable

Energy log

Disable

Digital outputs

Disable

Digital inputs

Input status

Pulse output

100 pulse/kWh, pulse width: 100 ms

Communication

Baud Rate = 19200; Parity = Even; Address = 1

Password

High: 0010; Low: 0000

Alarms

Disable

Front panel display LCD

Backlight: 4; Contrast: 5

Front panel display mode

Full screen: Enable; Auto scroll: Disable

Language

English

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.