DOCA0006EN-08

Setting the clock using the display

The following image illustrates how to set the clock when you initially power up the meter or after a power failure. To set the clock during normal operation, refer to the Configuration mode menu tree for your meter.
  1. Press when you are prompted to set the date and time when the meter is powered up.
  2. Use the or button to enter the meter Password (High) (Default is “0010”) and press .
  3. Use the or button to set the date in DD-MMM-YYYY format and time in HH:MM:SS format.
  4. Press to save your changes to the meter.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.