DOCA0006EN-08

Overview

The following settings can be configured in configuration mode:

Function

PM3200

PM3210

PM3250

PM3255

Wiring

CT and VT ratio

Nominal frequency

Date / Time

Multi-tariffs

Demand

Log

Digital outputs

Digital inputs

Pulse output

Communication

Password (High and Low)

Alarms

Front panel display

Language

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.