DOCA0006EN-08

Command Interface

Address

Register

Action
(R/W/WC)

Size

Type

Units

Description

PM3250

PM3255

0x1481

5250

R/W

R/W

1

UInt16

Requested Command

0x1483

5252

R/W

R/W

1

UInt16

Command Parameter 001

0x14FD

5374

R/W

R/W

1

UInt16

Command Parameter 123

0x14FE

5375

R

R

1

UInt16

Command Status

0x14FF

5376

R

R

1

UInt16

Command Result codes:

  • 0 = Valid Operation
  • 3000 = Invalid Command
  • 3001 = Invalid Parameter
  • 3002 = Invalid Number of Parameters
  • 3007 = Operation Not Performed

0x1500

5377

R/W

R/W

1

UInt16

Command Data 001

0x157A

5499

R

R

1

UInt16

Command Data 123

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.