DOCA0006EN-08

Set Date/Time

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

1003

W

1

UInt16

(Reserved)

W

1

UInt16

2000 – 2099

Year

W

1

UInt16

1 – 12

Month

W

1

UInt16

1 – 31

Day

W

1

UInt16

0 – 23

Hour

W

1

UInt16

0 – 59

Minute

W

1

UInt16

0 – 59

Second

W

1

UInt16

(Reserved)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.