DOCA0006EN-08

Input/output capabilities

WARNING
Unintended Operation
  • Do not use the meter for critical control or protection applications where human or equipment safety relies on the operation of the control circuit.
  • Be aware that an unexpected change of state of the digital outputs may result when the supply power to the meter is interrupted.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.