DOCA0270EN-03

Avatar Function Allocation

In the following table, a check mark ✔ indicates the function groups that are possible with each TeSys avatar.

WARNING
UNINTENDED EQUIPMENT OPERATION
Avatar current will be shown as 0 even though there is device level current when the current value is less than 10% of the FLA.
Make sure to select correct starter based on the load current.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Avatar Function Allocation – Protection and Monitoring

Name

Current Monitoring

Upstream Voltage Presence

Electrical Protection

Load Protection

Motor Overheat Protection*

Energy Monitoring*

System avatar

Switch

Switch - SIL Stop, W. Cat 1/2*

Switch - SIL Stop, W. Cat 3/4*

Digital I/O

Analog I/O

Power Interface without IO (measure)

Power Interface with IO (control)

Motor One Direction

Motor One Direction - SIL Stop, W. Cat 1/2

Motor One Direction - SIL Stop, W. Cat 3/4

Motor Two Directions

Motor Two Directions - SIL Stop, W. Cat 1/2

Motor Two Directions - SIL Stop, W. Cat 3/4

Motor Y/D One Direction

Motor Y/D Two Directions

Motor Two Speeds

Motor Two Speeds - SIL Stop, W. Cat 1/2

Motor Two Speeds - SIL Stop, W. Cat 3/4

Motor Two Speeds Two Directions

Motor Two Speeds Two Directions - SIL Stop, W. Cat 1/2

Motor Two Speeds Two Directions - SIL Stop, W. Cat 3/4

Resistor

Power Supply

Transformer

Pump

Conveyor One Direction

Conveyor One Direction - SIL Stop, W. Cat 1/2

Conveyor Two Directions

Conveyor Two Directions - SIL Stop, W. Cat 1/2

In the following table, a check mark ✔ indicates the function groups that are possible with each TeSys avatar.

Avatar Function Allocation—Predictive Alarms, PV, and Control Modes

Name

Predictive Alarms

Process Variable Monitoring

Configurable Control Modes

System avatar

Switch

Switch - SIL Stop, W. Cat 1/2*

Switch - SIL Stop, W. Cat 3/4*

Digital I/O

Analog I/O

Power Interface without IO (measure)

Power Interface with IO (control)

Motor One Direction

Motor One Direction - SIL Stop, W. Cat 1/2

Motor One Direction - SIL Stop, W. Cat 3/4

Motor Two Directions

Motor Two Directions - SIL Stop, W. Cat 1/2

Motor Two Directions - SIL Stop, W. Cat 3/4

Motor Y/D One Direction

Motor Y/D Two Directions

Motor Two Speeds

Motor Two Speeds - SIL Stop, W. Cat 1/2

Motor Two Speeds - SIL Stop, W. Cat 3/4

Motor Two Speeds Two Directions

Motor Two Speeds Two Directions - SIL Stop, W. Cat 1/2

Motor Two Speeds Two Directions - SIL Stop, W. Cat 3/4

Resistor

Power Supply

Transformer

Pump

Conveyor One Direction

Conveyor One Direction - SIL Stop, W. Cat 1/2

Conveyor Two Directions

Conveyor Two Directions - SIL Stop, W. Cat 1/2

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?