Internal Events
The following are potential internal events you might encounter during operation:
|
Asset Alarm |
|||
|
This alarm is triggered under the following conditions:
|
|||
|
Corrective Action: |
|||
|
Check the device diagnostics for each device. The one triggering the alarm is the one with the highest number of operations. Schedule maintenance to replace it. |
|||
|
Device Temp Threshold Alarm |
|||
|
Device temperatures are monitored by reading their internal temperatures. A device internal temperature alarm is triggered for a device if the internal temperature read exceeds its defined threshold. |
|||
|
Corrective Action: |
|||
|
Verify that the equipment design meets the ambient temperature requirements for the product. Cycle the island power. Replace the device if cycling power is unsuccessful in clearing the alarm. |
|||
|
CPU Load Alarm |
|||
|
Triggered when the CPU load read from the device exceeds 60%. |
|||
|
Corrective Action: |
|||
|
Cycle power. If the alarm is still present, contact your next level of support. The device may need to be replaced. |
|||
|
Avatar Alarm |
|||
|
A device within the avatar has experienced an internal event such as the following:
|
|||
|
Corrective Action: |
|||
|
Cycle power. If the alarm is still present, contact your next level of support. The device may need to be replaced. |
|||
|
Device Data Not Updated Alarm |
|||
|
Indicates a potential perturbation of communication between devices. |
|||
|
Corrective Action: |
|||
|
Verify that all installation guidelines are followed in the setup of the equipment. |
|||
|
Audit Record Capacity Alarm |
|||
|
The number of allowed audit records has been reached. |
|||
|
Internal comm loss (minor event) |
||
|
Corrective Action: |
||
|
||