DOCA0270EN-03

Starters and Power Interface Module (PIMs)

Device Status is the top LED on all TeSys island modules except the bus coupler.

Device Status LED

Indicator State

Summary

Description

Single Flash Green/Red

LED Diagnostic

Visual indication that LEDs are operational.

Steady Off

Off

Module not energized.

Steady Red

Device Major Event

Internal device event.

Flashing Red

Not Ready

Discovery, addressing, firmware update, Device Minor Event, etc.

Steady Green

Ready, Closed

Module is ready, and the contactor switch is closed.

Flashing Green

Ready, Open

Module is ready, and the contactor switch is open.

Load Status is the second LED on starters and PIMs.

Load Status LED

Indicator State

Summary

Description

Single Flash Green/Red

LED Diagnostic

Visual indication that LEDs are operational.

Steady Off

Off/Not Ready

Module not energized or not ready.

Flashing Green/Red

Test mode

System Test state is activated.

Steady Red

Protection Trip

Avatar Protection Trip.

Flashing Red

Protection Alarm

Avatar Protection Alarm.

Flashing Green

Upstream Voltage

No upstream voltage presence detected.

Steady Green

Normal

Load is operating within normal conditions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?