Setting the TeSys island IPv4 Address via OMT
Use this procedure to set the IPv4 IP address and gateway information on the TeSys island after you have connected to the bus coupler.
Once you are connected to the island, setting the IPv4 IP address and gateway information can be performed using the OMT.
Setting the Island IPv4 Address — OMT
|
Step |
Action |
|---|---|
|
1 |
Click the SETTINGS icon. |
|
2 |
Click the System avatar. |
|
3 |
Click FIELDBUS SETTINGS. |
|
4 |
Change the IP Mode to Fixed Address to manually set the IP address. |
|
5 |
Enter the Fieldbus IPv4 Address, Fieldbus Subnet Mask, and Gateway Address of the bus coupler. |
|
6 |
Enter the Network Name for the bus coupler. |
|
7 |
Click Save. |
|
8 |
Configure your PC with an IPv4 IP address and subnet mask in the same network that you recently applied to the bus coupler. |
|
9 |
Enter the new address (format: https://xxx.xxx.xxx.xxx) of the bus coupler into the web browser on your tablet to access the OMT running on the bus coupler. NOTE: The recommended browsers are Chrome or Safari.
|
|
10 |
Login to the OMT with the new password and verify the IP address has been successfully changed. |