DOCA0270EN-03

Energy Monitoring

Enable energy monitoring for each TeSys™ Avatar (except the system and device Avatars) as shown in the following table.

Enable Energy Monitoring

Step

Action

1

Click on MY AVATAR.

2

Click on each Avatar where energy monitoring will be used.

3

In AVATAR PARAMETERS, change the setting in LOAD ENERGY MONITORING from No to Yes.

4

Click OK to save the changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?