DOCA0270EN-03

SIL Interface Module (SIM)

NOTE: Safety Integrity Level according to standard IEC 61508.

Device Status is the top LED on all TeSys island modules except the bus coupler.

Device Status LED

Indicator State

Summary

Description

Single Flash Green/Red

LED Diagnostic

Visual indication that LEDs are operational.

Steady Off

Off

Module not energized.

Steady Red

Device Major Event

Internal device event.

Flashing Red

Not Ready

Discovery, addressing, firmware update, Device Minor Event, etc.

Steady Green

Ready

Module is ready.

SIL Status LED

Indicator State

Description

Single Flash Green/Red

Visual indication that LEDs are operational.

Steady Off

Module not energized or not ready.

Steady Green

No SIL Group Stop command.

Flashing Green

Successful SIL Group Stop command, not yet in SIL Stop State.

Flashing Red

Successful SIL Group Stop command, but indicative of a wiring issue. SIL Stop State achieved.

Steady Red

Successful SIL Group Stop command. SIL Stop State achieved.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?