DOCA0270EN-03

Restart System

If you need to restart the island, execute the Restart System command.

Perform the following steps:

  1. Click the Control Panel icon.

  2. Click Restart System.

    Result: The warning message is displayed on the screen.

  3. Read the warning message carefully and click OK.

    Result: The island restarts.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?