DOCA0270EN-03

Electrical Protection

Electrical Protection Settings Values

Setting Name Value Range Default Value Increment
Ground Current Trip Delay 0.1–1.0 s 1 s 0.1
Ground Current Trip Level

20–100%* FLA

50% 1
Ground Current Alarm Level

20–100%* FLA

50% 1
Current Phase Unbalance Trip Delay - Start 2–20 s 2 s 0.1
Current Phase Unbalance Trip Delay - Run 2–20 s 5 s 0.1
Current Phase Unbalance Trip Level 10–70% 20% 1
Current Phase Unbalance Alarm Level 10–70% 10% 1
Current Phase Loss Trip Delay 0.1–30 s 3 s 0.1
Current Phase Loss Trip Level 80% 80%
Current Phase Sequence
  • ABC
  • ACB
ABC
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?