DOCA0270EN-03

Verifying the TeSys island Configuration

Verify that all hardware is operating correctly and that all settings for the TeSys island, including the trip and protection notifications, have been configured.

Verify the Island Configuration

Step

Action

1

Visually inspect the bus coupler LEDs.

2

Visually inspect the power module LEDs.

3

Visually inspect the I/O and accessory module LEDs.

4

In SoMove software, verify that the configuration settings for the TeSys Avatar match the intended settings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?