DOCA0270EN-03

Phase Configuration

The Phase Configuration function applies only to single-phase TeSys™ avatars. In a single-phase system, this feature is automatically enabled. It triggers a Phase Configuration trip if the current in phase two is greater than 50% lr FLA for more than 1 s.

NOTE: Phase Configuration protection does not apply to three-phase operation.
@New in Draft1 V3
NOTE: TeSys island supports ABC and ACB phase configuration.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?