DOCA0270EN-03

Mounting Starters on DIN Rail

Before installing modules on the TeSys island, refer to the TeSys island topology to ensure you are installing them in the correct sequence.

To install a starter on DIN rail, position the top groove of the starter on the top edge of the DIN rail and press it against the rail until you hear the clip snap into place. See the figures below.

Size 1 (TPR••009) and Size 2 (TPR••025 and TPR••038) Starters (mm/in.)

Size 3 Starters (TPR••065 and TPR••080) (mm/in.)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?