DOCA0270EN-03

Configuring the Island Parameters

Settings are configurable for the system, load, and device Avatars to enable energy monitoring and to customize the Avatar settings. Refer to TeSys™ island DTM online help for assistance in selecting the settings. Press F1 while in the tool for help.

If the DTM displays the message "The system as configured using Modbus/TCP may result in a lack of data consistency for one function block input.  Please see the installation guide for more information." then one multi-byte function block input datum may be accessed by multiple Modbus/TCP PLC reads and could be incorrectly displayed in the function blocks. Use EtherNet/IP to ensure data consistency.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?