SIL Starters
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
For complete instructions about functional safety, refer
to the TeSys island Functional Safety Guide, 8536IB1904.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
SIL* starters provide similar functions to standard starters but are associated with a SIL interface module.
The main functions of the SIL starters are as follows:
-
Provide Stop Category 0 and Stop Category 1* functionality
-
Provide operational control for loads
-
Measure electrical data related to the load
-
Provide energy monitoring data when a voltage interface module is installed in the TeSys island
Multiple SIL starters might be needed for a single TeSys avatar function. For example, the avatar Motor Two Directions - SIL Stop, W. Cat 1/2* includes two SIL starters. In addition, avatars using SIL starters always include a SIL interface module.
The SIL starters are connected:
-
Upstream to a circuit breaker
-
Downstream to the load
The SIL starters communicate with the bus coupler, sending operational data and receiving commands.
SIL Starter Ratings
|
Power Ratings |
Amperage |
Reference |
|
|---|---|---|---|
|
kW |
hp |
||
|
4 |
5 |
0.18–9 |
TPRSS009 |
|
11 |
15 |
0.5–25 |
TPRSS025 |
|
18.5 |
20 |
0.76–38 |
TPRSS038 |
|
30 |
40 |
3.25–65 |
TPRSS065 |
|
37 |
40 |
4–80 |
TPRSS080 |
WARNING